Toolbars

  • New:

    Starts a new troubleshooting project

  • Open:

    Opens an existing troubleshooting project from file

  • Save:

    Saves the current troubleshooting project

  • Print:

    Prints the currently active view.

  • Cut:

    Current implementation the same as copy.

  • Copy:

    Copies the currently active view to the clipboard.

  • Paste:

    This feature has been reserved for future use

  • Histogram:

    The histogram of a selected field shows the frequency distribution of that particular field.

  • Trend:

    The Trend Tool allows you to view large (far in excess of 64000 data points) datasets as trends.   The typical use of the Trend Tool is to evaluate and edit your choice of upper and lower limits that have been assigned to a variable for Data Cleaning purposes.

  • Frequency Analysis:

    Use the frequency analysis to evaluate the frequency components of a time domain signal. This provides process information about events that occur at a particular frequency.

  • Scatter Plot:

    A scatter plot is a graphical view of the relationship between two variables.

  • Statistics:

    The Statistics View provides you with basic descriptive statistics of all the variables (fields) that were imported into Troubleshooter with the Data Import View.

  • Batch visualization:

    Details of all the selected fields for batch data are listed, enabling you to focus on comparing various parts of a product, batch, stage or similar.  By configuring any specific batch hierarchy as represented in a dataset, you are able compare any part of a batch process with any other part visually.

  • Pivot table:

    Select fields to create a pivot table of the data for analysis.

  • Export data:

    Exports the current active view.  Current views supported for exporting (export format included):

    • Trends (BMP)

    • Scatter plots (BMP)

    • Histograms (BMP)

    • Preparation view (CSV formatted text file containing all configured limits and delays)

  • Save blueprint:

    Exports the current project as an Action Object blueprint for editing in the Architect.

    (NOTE:  This option will NOT save the current Troubleshooter Project.)

Data Preparation toolbar

When manipulating datasets while preparing data for loading into the Troubleshooter projects, the data preparation toolbar becomes active. Use these toolbar options to visualize your data.


Related topics:

  

CSense 2023- Last updated: June 24,2025